Part Number: SN65HVD72
Hello,
I use the configuration see in the picture RS485.png.
The SN65HVD72 is the master and is always present, and after we can add 1, 2 or 3 MAX3483.
When I use only 2 MAX3483 and the SN65HVD72, it's OK, all work fine.
But, if I had a third MAX3483, I have a perturbation problem, this MAX3483 emit perturbation on the pin 1 (RO) and so the transmission don't work.
Do you see a mistake in my hardware configuration ?
Best regards