Part Number: TLK1211
Hi team
1. According to the top above specification, TXP-TXN is 600 ~ 1100mV.
Is this the value that makes High? Or is it the range of TXD?
In the figure second above, the value of VOD is between -1V and 1V.
0V is also 0 in absolute value. How is the range of 600 ~ 1100mV calculated?
2. In the figure above, the voltage values of TXP and TXN are not specified.
Transmit common mode voltage range is 1000 ~ 1400mV.
TXP = 1000 ~ 1400mV, TXN = 1000 ~ 1400mV Is this correct?
Thanks
TM