Part Number: TPD2S300
I am considering the use of the TPS2S300 into a different application for which it is originally intended. My customer has a single UART line (115kbps, 3.3V) that could potentially be shorted to a 22V line. I thought about using the TPS2S300 for protecting the system. My questions are:
1. Can I combine both CC lines into one and use it as the TX in the UART communication or should I leave one CC line open?
2. Do you see any problems with using this part for this purpose? Do you have a better suggestion?
Thank you!