Part Number: TSU6111
Other Parts Discussed in Thread: TS3USB221
Dear Team,
I sourced a part that can be a UART switch, could you help to confirm TSU6111 datasheet?
There are two output interfaces on TSU6111, one is USB and the other is UART, what if I would like these two interfaces are both UART, is it workable? ( if not please suggest a suitable one)
How about the driver, does it support linux or windows?
TSU6111 is designed to the mobile solution with charger function; for my application, do you have another part can meet my requirement, please recommend.
BR
Kevin