Part Number: TS5USBC41
Hi guys,
My customer is designing in the TS5USBC41 and would like someone from the product line to check their schematic and answer their questions:
Can youy review the following schematic and make sure it is acceptable?
A few questions.
Note: D- goes to D+ then D1+ goes to D-
D+ goes to D- then D1- goes to D+
Can FLT be left N/C without a termination resitior?
On the un-used output, TI recommends 50Ohm termination resitors.
Can I combine them into 1? Both C1 and C2, into R47?
Can we pull SEL1 and SEL2 direct to GND, I assume this isn’t an issue.
Thanks,
Brian