Part Number: DS250DF810
Hello TI team,
We are using DS250DF810 retimer device for one of our product design. So, presently I am performing signal integrity analysis for one differential PCB back plane channel. we were received IBIS AMI model for the same device. We are getting two different SI results at the RX side (i.e. after the post DFE, CTLE auto enabled equalisation) when we are configured "RX Config" as default i.e "1" and changed it as "0". Both the results are different. Can I know what are these RX config settings? which Rx config settings should we use for our simulations. Since by default settings signals are more noisy and results are very idealistic when we are configured it as "0".
Please can any one help us on this? It would be great if we can resolve these issues asap.
Thanks,
Naveen