Part Number: TPS65982
Other Parts Discussed in Thread: TPS65987D
Hi,
We are using TPS65982ABZQZR (USB Type-C™ and USB PD Controller Power Switch and High-Speed Multiplexer) as High speed multiplexer in one of our design.
As per datasheet, this device can also work as USB 3.0 power delivery controller. Can you please check and let us know if we can this device for Voltage negotiation over CC1 and CC2 lines of USB3.0/3.1 interface. Our module is operating as a device which is drawing power from HOST system. We would like to support a device which can negotiate for higher voltages (5/12/15/20V) over USB interface.
Please confirm the same.
Also, we are looking for a USB3.0 peripheral controller with I2C,SPI and GPIOs etc. Please suggest us available USB 3.0 peripheral controllers from TI.
Thanks & Regards,
Sunny Watts
Tel: +91-9999907724