Part Number: DP83867IR
Hello,
In design with the DP83867 Ethernet Phy and have a question about the input clock for the device. We are using a single ended LVCMOS 25MHz clock connected to pin 19. The datasheet does not specify the electrical requirements/properties for the XI/XO pins and we are wondering if that information is available. More specifically, we would like to verify that we can use a 1.8V LVCMOS clock for that input even though we have VDDIO set to 3.3V.
Thank you,
HSG