Part Number: DS90UB960-Q1
Tool/software: TI-RTOS
Hello,
My question is similar to what was asked in this forum before regarding register setting of UB960. I am using UB960-TDA2Px in radar satellite configuration. In the Vision SDK 3.5, in the "bsputils_ub960.c" file, referring to the defined table 'BspUtils_Ub960I2cParams gUb960Cfg_D3AR1243', you will see that the serializer I2C address is set in register 0X5D, I2C-SPI bridge address is set in 0x5E for all the receiver ports. This means that as per datasheet, the serializer is considered as SlaveID[0] and the radar sensor is considered as SlaveID[1]. If you refer the datasheet of UB960, you will see that SER_ID is defined in 0x5B and its alias is in 0x5C. Should I make an modification in the default register settings or should I consider the serializer as SlaveID[0]?
Thank you!
Best Regards,
Nishant