Part Number: DS16F95QML
Hi Team,
Our customer is using DS16F95QML-V device for one of the application. During normal operation, the device is wired in a card which is powered from a standard power supply. Last day, there was a power failure to the card and after that the device is not working normally. All other devices in the board are working correctly.
The device is configured with fail-safe mode. The AND voltage with respect to Ground is around 4V (High) and 1V (Low). After the power failure, the output voltage levels of AND reduced to 2.2V (High) and 1.25V (Low). However the NAND voltages are remain the same before and after.
What may be the reason for this failure. Please help with thoughts to analyse this issue.
Thanks in advance for your help and support.
Regards, Shinu Mathew.