Part Number: PCA9518
Hello team
I have two PCA9518s to configure 1:8 I2C expand like datasheet figure3. However I see comunication error with the configuration.
Looking at SCL1 of the device1, I found clock waveform has glitch like depression during high state.
When I don't connect each EXPSCLy, EXPSDAy and operate as 1:4, then the issue resolve.
Could you please suggest how to improve the behavior when operating 1:8 with using two devices?
Pullup resistor value what I use now is as below.
SDA0, SCL0: 10k ohm to 3.3V
SDA1-4, SCL1-4: 2.7k ohm to 5V
EXPSDA1-2, EXPSCL1-2: 6.8k ohm to 3.3V
Best regards,