This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: GPIO Event for disabling internal source switch

Part Number: TPS65987D

Hello,

does TPS65987D have a specific GPIO event for disabling the internal source switch? My implementation is like a notebook, Alt. mode, power sink 12-20V/5A, power source 5V/3A. I would like to control (enable/disable) the USB source switch in the system power states S3/S4/S5. I have checked document "TPS65987D GPIO Events" but there I found only "Sink Arbitration GPIO Input".

Thank you.

Best regards

David

  • Hi David,

    We do not have a GPIO event for this. However, you could open and close the sink switch through a Host EC by using the SRDY and SRYR 4CC commands. You could find more information on these commands in the host interface TRM:

    If this answers your question, PLEASE select This resolved my issue

    Thank you,
    Eric