Part Number: TUSB8044RGCEVM
Hi,
in section "2.6 power supply" of the operation manual (
) there are a few inconsistencies:
1. The description identifies J5 as the power connector while on the board this is J6.
2. The description says every downstream port can provide 900mA: 4x900mA = 3.6A
But the recommendation says that a 2-3A supply is adequate, this should be increased to ~5A or so.
Thank you!
Regards,
Alberto