Part Number: TPS65983B
Hi,
Is there a way to start a fresh project without loading any existing project templates (Add-in card, Apex, Bus-powered, Tahini or Tapex)? Currently We are looking a way to configure TPS65983B to work in a Thunderbolt device that has ~12Vdc internal supply, but no FETs to control input/output charging. In practice, the device would not source / provide energy towards host, neither it would consume/sink from it. Bus-powered device template would be the easiest, since we could make the negotiation where 5Vdc would be provided, even though not consumed. Apex/Tapex/Tahini are all adding either additional TPS65983B chip or FET controls due to mandatory charging option..