Part Number: TVS2700
Other Parts Discussed in Thread: TVS2701, TVS2201
Hello,
I would like to use the flat clamp devices with a +48VDC supply. Can I stack two of the TVS2701 (Vrwm would then be 54V) in series as with stand TVS devices? I realize the dynamic resistance will double, but power dissipation should be the same in each device. Is there any reason you would recommend against this?
Thank you