This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: Input on valid power down conditions of PCA9306 as isolator for I2C slave

Part Number: PCA9306

Hi,

I am interested in using the PCA9306 (assuming that this is indeed my best option) to isolate an I2C bus from an I2C slave. I'm designing a low-power system where I want to be able to individually isolate and power down various sensor nodes that are not in use. I would like to confirm whether it is ok or not to hook the EN signal of PCA9306 to the SLAVE VDD and then power down the entire slave supply. When the slave is enabled, the voltage levels on each side of PCA9306 will be the same. See figure:

Does this seem ok to do?

Thanks!