Hi everybody,
I am trying to make a design where a camera with CSI-2 interface must be connected to the related receiver.
Unfortunately I can't have a straight and short connection between camera and receiver, since there are 20 or 30 cm of traces on different PCBs where the signals have to pass trough.
Perhaps, due to some reason, the impedance between two different PCB is not perfectly matching the impedance of the whole line.
So I was thinking to use some buffer/repeater for the CSI-2 lanes (1 clock and 4 data lanes).
I still don't understand what is I need a dedicated buffer, or if any general purpose lvds buffer is ok. I am really confused.
Can anyone help me ?
many thanks in advance
Stefano