This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042-Q1: select new part number for package reason

Part Number: TCAN1042-Q1
Other Parts Discussed in Thread: AWR1843BOOST,

       When testing AWR1843boost demo, because of the package reason, they want to use 3mm*3mm CAN device. So the recommended model number is in the TCAN1042-Q1 series. Could you please help to select the part number? And the CAN device need to meet the requirements as follows.

  1. Package: 3mm*3mm;

  2. Meet AEC-Q100: Qualified for Automotive Applications;

  3. Support 5Mbps rate CAN FD;

  4. Support hot swap;

  5. Supply: VCC 5V/VIO 3.3V