Part Number: TPS65982
Hi Sirs,
My customer used two TPS65982 and shared external flash to desgined a Dual-Port Notebook application without DC barrel jack.
First, they used one 45W USB-C adapter to provide power source to system and battery charger.
After 45W adapter provided power to system working well, they also used one 65W USB-C adapter to provide power source to anther port.
They found the TPS65982 still choose 45W adapter to provide power source to system.
A few questions as below.
1. Why the TPS65982 didn't have to choose highest power source? may I know the GUI setting can to fix it? or need the EC to control TPS65982 to choose the power souce path?
2. My customer would like to read the PP_EXT path current data from register, how to get them?