Other Parts Discussed in Thread: EV2400, MSP430F5529, BQSTUDIO
We have an issue on few of our EV2400 purchased a year ago which was not used. We purchased 9 of them, 5 of them works fine without any issue.
4 of them have issues.
Here’s the issues we encountered:
- With the EV2400 connected, power up the PC. Run the BQ Studio or BQ EV Software, it cannot detect the EV2400.
- Remove/re-Insert USB cable to EV2400, Run BQ Studio or BQ EV Software, it works.
Another Scenario using Devcon:
- With the EV2400 connected, power up the PC. Run DEVCON.EXE (to initialize or reset the USB port for EV2400)
- Running the BQ Studio or BQ EV Software, it cannot detect the EV2400.
- Remove/re-Insert USB cable to EV2400, Run BQ Studio or BQ EV Software, it works.
Another Scenario using Reset button:
- With the EV2400 connected, power up the PC. Running the BQ Studio or BQ EV Software, it cannot detect the EV2400.
- Press Reset Button of EV2400, Run BQ Studio or BQ EV Software, it works.
We tried the 5 EV2400 that’s working, it works constantly without issue.