Part Number: SN65DP149
Dear all,
Whether the SN65DP149 can be used for hdmi-to-hdmi design, which is equivalent to the use of an equalizer for HDMI.
I see that there are reserved HDMI interfaces in the sllu232 reference design, but there is no detailed description.In addition, I want to make compatible design, choose DP and HDMI at the input side, and choose HDMI at the output side.
It is ok? Looking forward to your comments;