Part Number: DP83867IR
I am using the DP83867IRPAP part in 100Base-TX mode. According to the spec and like other PHY's, the TX and RX clock are driven from the PHY. I have hooked up my part using external straps to auto neg and the other side is telling me its connected at 100. I do show the link led is active on the part as well. the RXCLK, Enable and Data work but the TXCLK is not outputting any clock or enable or data. The spec is somewhat confusing since some pics show the TXCLK as an input to the PHY in the Functional Block Diagram on Page 25. Don't see an errata on this either. Can anyone help on this...