Part Number: TPS65982
Hi,
I have used DRP prefers host template with the following changes to template configurations:
- In control registers I have enabled Process swap to UFP and Initiate swap to UFP and disable Process swap to DFP / initiate swap to DFP
- I have two PDOs in TX sink i.e 5V/0A and 20V/3A
- I have verified register settings with Host interface utilities tool.
- In Port information under System Configuration I have "Toggles R_p/R-d on CC ( with trySrc) , supports data/Power role swap
- PP_5V0 switch configured as swtich output enabled
- PP_HV disabled.
- Enabled GPIO_1 for event "Allowed (Active low) event and GPIO_2 for event "Cable orientation"
Our requirement are as follows:
1.is to act as as a sink with PD negotiation of 20V.3A capability.
2. Also be a UFP device when connected to a PC
3. No DP or Intel VID
3.USB gen 2 and Gen3 supported
I have attached my project with this email. Please let me know soon as this is urgent. TPS65982 HD3SS460 DRP, Prefers UFP Sink.pjt
Please let me know if making any protocol violation.
regards,
Ali