Part Number: SN65HVD256
Other Parts Discussed in Thread: TCAN337, TCAN330, SN65HVD234, SN65HVD230
Hello,
Our customer use the SN65HVD256 with the VRXD as 3.3V.
The customer are considering a new project. They will use the supply voltage as only 3.3V.
They are looking for the CAN transceiver with same function as the SN65HVD256 except for the VRXD pin.
Do you have any recommend device?
The application of the customer is not automotive. So they do not need Q1 grade.
Best Regards,
Naoki Aoyama