Part Number: SN65DSI84
Tool/software: Linux
Parameters of the panel:
Resolution: 1600x1200
Vertical Period: 1233
V-Blanking: 33
Horizontal Period: 880
H-Blanking: 80
Panel clock: 65.125Mhz
Test pattern shows normally but only half of the screen shows up in non-test mode.
In addition, nothing shows up if the 0x20 and 0x21 registers are set to 1600 in non-test mode, the half screen is seen when 0x20 and 0x21 registers are set to 800.
Attached are the DSI status and CSR files generated by the DSI Tuner V2.0.
What are not set properly?