Part Number: TCA9803
Hello
Below is customer question.
a) Could TCA9803 A side connect with PCA9511?
b) Master Vcc, TCA9803 buffer1 Vcca, buffer2 Vcca use different 3.3V power rail, is it ok?
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9803
Hello
Below is customer question.
a) Could TCA9803 A side connect with PCA9511?
b) Master Vcc, TCA9803 buffer1 Vcca, buffer2 Vcca use different 3.3V power rail, is it ok?
BR
Patrick
Hey Patrick,
A) A side should work. One thing to note is A side of TCA980x has a deglitch filter which turns on when you pull A side low temporarily, typically you do not see this on an o-scope unless your VoL on A side is larger enough. You may see TCA980x drive the line low for some nano seconds when you use this device with something with a dynamic offset like PCA9511. This is normal behavior and i do not expect any problems.
B) This is also okay. TCA980x is meant to be high impedance when the power supply is not present.
Thanks,
-Bobby
Hello
1. Per Fig 1, does the topology have any problem for it?
2. Per Fig 2 topology, A side of TCA9803 connect to input side or output side of PCA9511 has no problem, right?
3. Per Fig 3. , if TCA9803 B side-B side connect with PCA9511, has any risk for it? salve EXP1/EXP2 independently communicate with BMC master. Thank you.
Fig 1
Fig 2
Fig 3
Fig 3
Hello
Some questions below also.
1.As B side with internal pull up ,there will be two pull up resistor respectively to different power(P3V3_EXP1,P3V3_EXP2) when B side connect with B side, is it ok?
2.Is this topology connection be effective for isolate P3V3_EXP1,P3V3_EXP2, P3V3_STBY?
3.PCA9511 has rise time accelerater (we only use PCA9511 hot swap function, don't need repeater function),B side connect with it, ok?
BR
Patrick