Part Number: DS90UB913A-Q1
Dear support team,
I am using DS913/4 SER-DES pair. With SER 913 I am facing one issue. In certain fault condtion as per requirement it is expected to RESET the microcontroller. In this scenario I see 3.3V powersupply is not going to zero completly and returns from 0.8V to 3V3 again. In this situation SER 913 become unresponsive and we can not establish the link with DES. This situation not recover even if we try to toggle PDB pin of SER.
This become a stuck situation of SER from which it never recovers, can you please suggest a solution on this?
Thanks and Regards
Rajan