Part Number: TMDS181
Hi,
Our boards are currently using the TMDS181 as part of the HDMI solution on the sink side.
My question is regarding HDMI2.0 mode, when it goes into retimer mode.
1. How exactly does the TMDS181 recover just the clock? From the datasheet description, it sounds like there is a CDR on the CLK input pin only, and it uses that recovered/clean clock to sample the data on the RX0/1/2
2. The second question is the REV_ID read back from address 08h, we see the same revision 1 as mentioned in the datasheet. Is this the latest silicon rev?
3. We are seeing HDMI compliance failure following the recommended use model, failure is on RX1 pin only with the intra-pair test start to fail at 0.6Tbit skew (negative) in debug mode. The compliance test limit is ~0.7Tbit. No issues when positive skew is applied. RX0/RX2/CLK lanes all pass the test and our board trace intra-pair skew is within 1ps from simulation.
the datasheet has a parameter Tsk_intra (output skew) from the TMDS181 which is 0.15Tbit, which is roughly about 25ps in 4K mode. Is my understanding correct that regardless of the input data skew, the TMDS181 will always provide an output under this datasheet limit? (obviously there would be bit errors if the input data skew is too large)
Thanks,
Xi