Part Number: SN65HVD3088E
Other Parts Discussed in Thread: THVD1550
Hi,
I'm a bit of a DIY novice, but I was wondering if I could use the SN65HVD3088E to transmit SPDIF (digital audio) at 192khz 24bit data over a twisted pair in a cat5 cable and then re-establish a single ended SPDIF signal at the other end? Ie one as a transmitter and the other as a receiver.
My concern is that the original SPDIF signal is only 0.2-0.6v, so would it 'trigger the transmission threshold' (if you get my meaning)?
If it would work, I'd then like to 'split' the original twisted pair into two equal ones (Left and Right signals) and feed it in to 2 SN65HDV3088E receivers - so the stub (that is referred to at the end of the data sheet) is not really a stub at all.
Would this require equal termination resistors of twice the normal value so the transmitter still see them in parallel and therefore the correct impedance (I'm guess about 100 ohm, so that would be 200 ohm at the receiving end of each twisted pair).
Many thanks,
Trevor