Other Parts Discussed in Thread: TIDA-050014
Our TPS65987D is configured as a sink design with a SPI flash for configuration (similar to TIDA-050014). The flash is programmed for the default 5V contract and a 15V contract. The USB_D+/- signals are intentionally not connected to the TPS65987D in our design because we do not want to support 5V charging in our application.
When we connect to a USB-C charger, the 15V contract is made and we see the PP_HV1 output start at 5V, then ramp up to 15V like it should.
When we connect to a standard USB 2.0 port on a PC, we get inconsistent behavior as follows:
1) Sometimes the PP_HV1 stays at 0V, which is what we want.
2) Sometimes the PP_HV1 quickly switches on immediately and produces 5V.
3) Sometimes the PP_HV1 starts at 0V, then 5-10 minutes later switches to 5V for an unknown reason.
When PP_HV1 is at 5V, I used a programmable load to see how much current was available. I was able to draw up to 2A from PP_HV1 before the power switch tripped. Once the load was removed, the PP_HV1 eventually returned to 5V.
Is this behavior normal? Is there a way to guarantee that PP_HV1 remains off when connected to standard USB ports?
Thank you,
Chris