Part Number: DS90UB948-Q1
The DS90UB948 datasheet on page 26 describe the "Maximum Repeater application". it says that "Two levels of Repeaters are supported with a maximum of three Transmitters per Receiver".
I need to have a one trasmitter to one receiver configuration, but I need more levels than two (up to 10).
It's the DS90UB948 support this configuration?
This limitation is due to I2C addressable number of devices?
I not need the remote (passthrough) I2C functionality... every device couple (SER/DES) will be managed locally by a MCU.
Thank you in advance.
Giuseppe