This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB927Q-Q1: Question about DS90UB927Q-Q1

Part Number: DS90UB927Q-Q1
Other Parts Discussed in Thread: DS90UB928Q-Q1

Hi Team,

I have question about DS90UB927Q-Q1 and DS90UB928Q-Q1. 

-Is it possible to transfer the image signal of 1280*800?

-Could you tell me the biggest image size to be able to transfer?

According to the datasheet, It is possible to support 5MHz-85MHz pixel clock on the devices. therefor it is possible to use 81.9MHz DCLK frequency from TFT LCD interface right?  

I am awaiting your reply.

Thanks,

Masayuki