Part Number: TPS65987D
Hi,
I'm designing my board from the TPS65987-90EVM circuit. The EVM board adopt an FTDI chip to configure the TPS65987D, but I'll eliminate the FTDI and place a connector which pins connect to SPI and I2C of the TPS65987D. I'm going to use the Aardvark adapter to configure through the board connector. I summarize my questions;
1. Where can I buy the Aardvark adapter?
2. Figure 23 of the SLVUAR8A document describes the I2C connection only, while the FTDI on the EVM connects both I2C and SPI. Is the I2C sufficient for the configuration and programming?
3. Figure 23 says you connect I2C port 1, while the EVM FTDI uses I2C port 2. Which is correct, I2C port 1 or 2?
Thanks again,