Hi Ti experts,
Previous ,we have used DP83822IF in100M-TX mode , the function is OK. now , we are using DP83822IF in 100M-FX mode, there is a packet loss in first few packet, then I read the link status of register 0x0001(bit 2), 0x08 is the PHY address of one port, before I read it,the fiber connection is OK, the first value is 0x7849, that is to say, the link is not eatablished, but after the first time I read it, the link status is OK ,
I don't know why the first link status is abnormal? thanks for your help