I am developing video system. For my application there is a need to split MIPI CSI-2 video signal on two (all units are on one board, there are no connectors on this path), so each processing unit can grab it.
Is there any special ic for that or is it possible to split each line of CSi signal on two and push each of them to SN65DPHY440SS, so it will buffer and clean each of them?