Part Number: DS90UB949-Q1
Hi,
I have a query regarding the GPIO register configuration of ds90ub949-q1 serializer.
I wanted to configure PIN 11, D_GPIO2 as input as well as PIN 5, GPIO1 as input. I understand that I have to set the register 0x0E = 0x33. But how do I select between D_GPIO2 ( bit[7:4] ) and GPIO1(bit[3:0] ) if i have to set PORT1_SEL = 1 to select D_GPIO2?