This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: can you confirm CSI-clk is independent from the synchronization mode ?

Expert 7280 points

Part Number: DS90UB953-Q1

Dear team,

Can you confirm the CSI-clock (on CSI_CLKP/N) can be anywhere between 40MHz and 416MHz to support 80 to 832Mbps CSI data rate per channel ?

Can you also confirm the CSI-clock is independent from the synchronous/non-synchronous mode we select ?

Typically in my application, 953 would be in synchronous mode, and the CSI-clk would be 324MHz.

Thanks a lot in advance for your confirmation!

All the best,

PA