Part Number: DS90UB948-Q1EVM
Dear Support team,
we are facing a poblem while trying to display a video on a LCD screen, using the Serdes products.
The configuration is as follow:
- Deserializer DS90UB948 (EVM)
- Serializer DS90UB949 (EVM)
- 1-Lane mode, using 1 coax cable
- video source: HDMI output from a PC
- Display: LCD Screen 1280x800 RGB 60fps
We attach pictures to illustrate HW configuration and parameters (DIP Switches for Mode SEL0/1)
The registers are forced to Coax mode and Single Link but it seems that there is a conflict. The register keeps changing from single to dual link mode automatically. (Unfortunately, we can't find how to upload .txt files which should be useful to upload the local and remote registers....)
The image is not "fixed", Lock LED keeps blilnking. We face the same behaviour with the pattern generated by the EVM.
EDID configuration generated from these parameters:
pixel_clock : 71.1 h_resolution : 1280 v_resolution : 800 h_blanking : 160 v_blanking : 23 h_back_porch : 80 v_back_porch : 10 h_sync_width : 32 v_sync_width : 3 h_size : 21 v_size : 13 d_gamma : 2.2
Have we missed anything ?
Thanks for your precious help.
Best Regards,