Part Number: DS90LV049Q-Q1
「English」
About electrostatic test
An electrostatic test was performed on the cable connected to the RIN 1 - / +, RIN 2 - / + terminals of the "DS90LV049Q - q 1", and the ROUT 1 and ROUT 2 terminals are fixed at H level.
Please tell me the countermeasure method.
「Japanese」
静電気試験について
”DS90LV049Q-q1”のRIN1-/+、RIN2-/+端子に接続されたケーブルに対し静電気試験を行ったところ、ROUT1、ROUT2端子がHレベル固定となります。
対策方法を教えてください。