Other Parts Discussed in Thread: SN65HVD234, TCAN332
Hi teams,
I have a question about SN65HVD234.
Please let me know about the follows.
The device is driving in "1" state.
I think it is in Hi-impedance, so it has driven somewhat.
In TCAN332, it is stuck on "1" state with the same circuit.
I think that the difference between these two devices is in the internal structure, is not it?
Best regards
Hayashi