Part Number: DP83822HF
Other Parts Discussed in Thread: USB-2-MDIO, MSP430F5529
Hi Support team,
I have a problem to connect with the microchip switch IC ( KSZ8863 )。 We would like to know if the PHY IC ( DP83822HF ) config as RMII interface as below table mentioned.
if no connection of MDC and MDIO pins? Does the PHY IC can work fine or must be connected those pin for control.
And
How about the below configuration for RMII interface is correct or not
Pin Mode RH RL
COL 4 open ( NC ) open ( NC )
RX_D0 1 open ( NC ) open ( NC )
RD_D1 1 open ( NC ) open ( NC )
RX_D2 1 open ( NC ) open ( NC )
RX_D3 1 open ( NC ) open ( NC )
LED_0 4 open ( NC ) open ( NC )
CRS 2 13 kOhm 1.96 kOhm
RX_ER 4 open ( NC ) open ( NC )
RX_DV 4 2.49 kOhm open ( NC )
Regards
Kelvin Lo