Part Number: ONET1151L
I am trying to use the ONET1151L in a new design. I have used this chip in the past and used the eval board schematic as a basis for my project's design. Using that schematic I have had no performance issues.
For the new design, I need to pack this laser driver into a very tight space. In the eval board schematic, there are a number of components on the outputs of the laser driver referred to as "bias tees". They are made up of a 475 Ohm resistor in parallel with a 47uH inductor, and this combination in series with a BLM15HG102SN1 ferrite bead. Given my space constraints, I was wondering if I could remove any of these components and have the ONET1151L still function and perform at 10G? Since they are "bias tees" I assume the 475 Ohm resistors need to be there. My question is, can either the 47uH inductor or the ferrite bead be removed or at least downsized to a smaller device? The other question is, if I remove them, what impact would there be on the output performance of the laser driver? Any help here will be greatly appreciated.
Thank you,
Mike Nycz