Part Number: TVP5150AM1
Dear Sir,
If use s-video to do input signal, output signal is BT656.
May I refer datasheet's application circuit(page-75) to do design, Please you kindly provide suggestion.
Thanks
Steven
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TVP5150AM1
Dear Sir,
If use s-video to do input signal, output signal is BT656.
May I refer datasheet's application circuit(page-75) to do design, Please you kindly provide suggestion.
Thanks
Steven
To configure for S-Video please refer to section 3.21.1 in the datasheet.
Register 00h controls the video source type and channel selection.
For S-video set bit 0 = 1. Bit 1 does not matter when S-video is selected.
When S-video is selected input 1A = luma and 1B = chroma.
BR,
Steve