Part Number: TUSB1310
Hi dear supporting team,
for TUSB1310 layout, customer has below questions on trace control:pls help on it, tks a lot!
1. TX(ref to TX_CLK) and RX(refer to PCLK), should they do equal trace independently?
2. TX_DATA&TX_DATAK and TX_CLK need do equal trace, what's the length difference could be? is there other signal need be equal to TX_CLK?
3. TX_DATA, TX_DATAK and RX_VALID need be equal with PCLK, what's the length difference could be? is there other signal trace need be equal to PCLK?
4. TX_CLK and PCLK trace need be qual, is there skew requirement?
5.should they do equal trace length for control and status signals? if yes, which clk should be the reference?
and BTW, for the JTAG related pins, if they do not use it, could they float them? tks!