Part Number: DP83865
Hello,
we are using the DP83865 on custom designed interface cards since 2010. The design didn´t change since then.
We are using many interface cards in a machine for real time data transfer. Speed is always 1000MB/s. The interface cards are directly connected to network-cards in a PC.
We never had this problem before, but now in a new machine we have sometimes an issue with the data transfer.
On some of the cards the active link is suddenly disturbed and no data transfer is possible anymore.
The links is not recovering by itself! We have to un-/plug the cable, reset the PHY or do a power-cycle on one of the link partners to reestablish the link.
When the issue happens:
- the Link is still active -> LINK1000_LED is still on, and the corresponding registers are set.
- the activity LED is flickering weakly
- in the 1000BASE-T Status Register (1KSTSR address 0x0A) idle-errorcount is always 255 , also in subsequent reads. Local Receiver status is OK, Remote Receiver Status is sometimes NOK
- the issue happens when PHY is in master or slave mode
Apart from this issue we don´t see a problem with the data transfer. There are no lost packets before the link is disturbed.
As i see it, a disturbance on the cable/link should only cause some lost packets.
What can cause this problem that the link is not recovering by itself?
Thank you,
Best regards,
Markus Anders