This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1046A-DCI: TUSB1046 configure EQ resistance

Part Number: TUSB1046A-DCI

Sorry to bother you, as shown below EQ control pin internal pull-up 35k ohm & internal pull-down 95k ohm & four level setting i only knows these messages, but when TUSB1046A default I2C to enable then the default of EQ control pin is internal pull-up or pull-down resistance?

Thank you!

Best regards,

Yu hung.