Part Number: DS90UB913A-Q1
Other Parts Discussed in Thread: DS90UB913Q-Q1,
I am using a OVM6946, 400 x 400 camera with a OV426 interface IC. I am using the serializer's external clock at 48MHz and returning 24MHz to the OV426. I have two questions: First, if there is no pixal clock initially, does the serializer still establish the FDP-III link as it claims on sheet 23 on the data sheet? If so, what would be the expected frequency? I am not seeing it with the oscilloscope. Second, the pclk is only 8MHz. Is that a problem?