Part Number: TLK10232
Hi all,
My customer is working on initializing the TLK10232 for their environment. They are following the tlk10232_BringupProcedures_v2.pdf that is marked Ver 2.0 - January 2013, and "preliminary - subject to change".
Is this the most recent version of the bring up document? If not, could you provide a link to the most updated document?
The customer noticed some potential typos as described below:
In the section titled:
KR using manual mode settings learned from Link Training, with 156.25 MHz / 312.5 MHz Refclk
There is a subsection called:
Default HS Tx settings loading and LT controls
Within this section are the following instructions:
“o Write 16’h2000 to 7.0
o Write 16’h0000 to 30.150
o …
o Write 16’h0002 to 30.150
o Write 16’h1C00 to 30.36869”
This appears to be disabling the start-up protocol for Link training and then later re-enabling the startup protocol.
However, that should be done by writing to Device Address 0x01 instead of 30 (0x1E).
Device Address 0x1E.0x96 (30.150) isn’t referenced anywhere in the TLK10232 datasheet.
As mentioned above, DeviceAddr.Reg 0x1.0x96 (1.150) is defined in the LT_TRAIN_CONTROL section of the tlk10232 datasheet.
Are these instructions correct?
Thank you,
Jon