This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DPHY440SS: RSTN and VREG_OUT are unexpected low

Part Number: SN65DPHY440SS

Hi,

Is there any reason that RSTN and VREG_OUT are still 0V after 1.8V is applied at Vcc with below design?  

  • RSTN is only connected to GND through a 0.22uF cap.
  • VREG_OUT has two 0.1uF cap and being connected to VDD pin with two 0.1uF cap.

What can be checked further to clarify this?

Thanks!

Antony