Part Number: DS90UB953-Q1
953 input: MIPI-CSI Data 2MP/60fps + Voice(8K or 4K sampling Rate)-TDM or I2C
1. Could we use the GPIO of DS90UB953/954 to transfer the Voice data-8K/4K sampling rate?
2. How about the Max speed for the GPIO?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953-Q1
953 input: MIPI-CSI Data 2MP/60fps + Voice(8K or 4K sampling Rate)-TDM or I2C
1. Could we use the GPIO of DS90UB953/954 to transfer the Voice data-8K/4K sampling rate?
2. How about the Max speed for the GPIO?
Hi Kim,
from the GPIO rate spec., it is well to transmit 8Kbps signal. regarding the maximum speed of GPIO, can you check the d/s on GPIO description which has GPIO rate and jitter description. you can get to know the GPIO feature of UB953 better.
best regards,
Steven